Good morning,
I am currently an undergraduate student at the Democritus University of Thrace in Greece performing my dissertation thesis in the field of biomedicine. For this purpose, my colleagues and I, would like to develop a system of wearable sensors that will enable the continuous monitoring of vital biomedical parameters such as the body temperature, the blood pressure, the saturation of oxygen in blood, the hearth rhythm, as well as the electrocardiogram.
Based on past projects, I have in my disposal the products, but I do not know for sure if this is the appropriate for the conduction of the system as described above. To a greater level of detail, I have already the following products:
- ADS1293EVM
1) For this reason, I would like to take some measurements to become more familiar with ads1293evm and to understand more how it works and provide information regarding the electrocardiogram. So I would like if you could tell me which electrodes and wires-cables to take that will be compatible with ADS1293 to perform my experimental measurements. ( if you could i would like to suggest me companies which have warehouses in europe or companies such as Mouser, Svtronics). I want to suggest me specific components or sites in order to purchase them quickly
2) I want also to purchase An ECG SImulator , so i would like also to suggest me one ECG SImulator accordind to the above.
Kinds Regards
Sotiris Katsimentes