Hi,
I'm looking at the datasheet for AMC1106x and in the typical application section it shows that the shunt resistors can be connected to the hot lines.
Also in the datasheet mentions that the voltage that can be on input pins of the IC is couple of volts.
I was wondering if I can put the shunt resistor on the hot side with voltage of 48V or 240v bus or it has to be on the low side?
Thanks in advance