This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC53401-Q1: VOL information of SDA

Part Number: DAC53401-Q1
Other Parts Discussed in Thread: DAC53401,

Hi team,

DAC53401 outputs LOW for ACK, but there is no description about Vol specification of SDA pin in the datasheet.

I believe it has Vol(max)=0.4V capability at IOL=3mA the same as other I2C device.

Could you make sure the Vol specification for DAC53401-Q1? It needs the calculation for the pullup resistor.

Regards,

Saito