Hello. I have been using the LMP92066 in a few IRAD programs and now hopefully in production hardware. In two boards the -5V pin has shorted (1.7 ohms) and the devices are drawing excessive DC current. Those devices are now damaged. Is the device turn on dependent on power supply sequence? Should I turn on -5V first, then +5 or +5V first and then -5V? Your help is appreciated.