Other Parts Discussed in Thread: ADS1274,
hi,
My design daisy chains 3 ADS1274 in dynamic mode. I want 3 channels from each device, so channel 4 is powered down - permanently with on-board connections. It runs in Low Power Mode, ADC and SPI clocks are 5.12 MHz. Want to use the EVM boards to get a head start on code development. Our processor is STM32L.
I have 3 ADS1278 EVM systems. How can I daisy chain these and then connect to the STM32L SPI? Mostly interested in routing power to the 3 ADS1278EVM-CVAL's properly and powering down channels 4 thru 8. Can I do all this with jumpers? Do I need all 3 MMB0?
Don't need a detailed connection drawing. Just to know if what I want to do is possible and any tips to help me along.
If daisy won't work, I could just take 8 channels from a single EVM. Not the 9 I want, but other than that, would there be any difference apparent to my STM code?
mark