For an application where the ADS1259 operates on a single +5V supply and the REFOUT (+2.5V) is tied to the AINN pin.
If a low pass RC filter is placed before the AINP pin with R=50 Ohms and C=10nF (fc = 159,155 Hz), would this basically provide an anti-alias filter at all sample rates (10 Hz to 14,400 Hz) because the ADS1259 is oversampling at 921,600 Hz (fclk/8 where fclk = 7.3728MHz) and implementing digital low pass filtering?
Would a low pass filter cut-off frequency of 460,800 Hz or lower provide a universal anti-alias filter for all sample rates (10Hz to 14,400 Hz)?
What is the lowest low pass filter cut-off frequency (or the highest RC value combination) that can be placed in front of the ADS1259 inputs without using a buffer between the low pass filter and the ADS1259?
Thanks