Hi Team,
Our customer reported that he is using DAC7760IPWP during 2 years for industrial DAC device but a few weeks ago he found some error on the output. According to our customer,
When he sent to setpoint to 33.33% to our device, voltage out measure to Zero. normally it has to be out 1.666V because the device work on 0~5V range.
So I tested it with 4 DAC7760s.
All four chips had identical test results.
It shows the same symptoms when you request output in the same specific section.
I already made 200 Boards for our products.
Attached is the schematic diagram.
Regards,
Danilo