This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3664: Are there any distributors you can recommend from ADC?

Part Number: ADC3664
Other Parts Discussed in Thread: THS4551, , THS4541

This is a process in which the infrared signal passing through the photodiode and external noise must be input to the FPGA through the ADC.

In the case of a high-performance ADC, the input is differential. Does TI have an IC that divides the input signal 180 degrees differentially?