Other Parts Discussed in Thread: DAC60504, , DAC80504
I would like to ask the question of using DAC80508. First, let me explain that we have been using DAC60504 originally, and all the controls are smooth and normal.
Now the same project needs to be changed to DAC80508 (actually only need to use OUT0~OUT3), but there are problems in use, " Unable to read the device ID ".
Main control IC : STM32F411
Because the OUTX of the DAC80508 cannot be controlled, the DEVICE ID cannot be obtained by reading the DEVICE ID. So Need TI tech team to help me out for it.
The ID value read back is all 00 (the same FW setting can read the ID in DAC60504).
I don't know if there is any special attention to it? Or is there a related demo code?