Hallo everyone,
I need to interface the ADS9110. Our hardware developer wired the ADC like described in chapter 7.5.4.2. (Single Device: Minimum Pins for a Standard SPI Interface)
But when reading the chapter 7.5.2 (Interleaving Conversion Cycles and Data Transfer Frames) it's stated that:
"To achieve the rated performance specifications, the host controller must ensure that no digital signals toggle
during the quiet acquisition time (tqt_acq) and quiet aperture time (td_cnvcap) [...]"
Furthermore all timing-diagramms in this chapter show, that the CS goes low after td_cnvcap.
Isn't the connection between CS and CONVST breaking this rule?
What are the consequences regarding performance, when connecting CS and CONVST?
Thanks and regards,
Marcel.