I have a design in which I use the DAC122S085 to set the current limit for a motor drive.
The design seemed to work great but I have been running into issues when testing at -40C. Basically, the DAC is commanded an output on boot up, thus setting the current limit. This current limit is set at boot up and never really touched again. What is odd is the DAC output drops to 0V after attempting the first move from a cold start. If I command the DAC with a new output value after it has an output of 0V it seems to maintain that output.
At first was thinking it may be a software error but no evidence of that. Then I thought the DAC may be rebooting if the 3.3V was drooping at all, but it appears to be rock solid.
I have attached a capture (albeit a bad noisy capture as my measurement setup is non-ideal), may try to make a better setup for tomorrow.
Thought I would post on here to see if there are any other ideas of what may be going wrong. I am hitting a wall in the debugging process. I am going to get better captures later today or tomorrow.
Yellow: 3.3V Rail (Across the DACs Capacitor)
Green: Chip Select Line
Blue: DAC Output
Pink: CLK
Thanks.