Other Parts Discussed in Thread: ADS1299
I'm having problems reading data from the ads1299 eeg board, specifically the device id. I'm getting 0, and I'm
assuming that this is because I'm not properly powered up and/or jumpers are incorrect.
First question, Is there any difference in powering via 3.3V, vs 5V? I'm currently using 3.3, with a raspberry pi 4.
Second question, what is considered pin 1 on block J3 when looking at the board? Is it the circled pin in the below image, or
the pin behind it?
Current jumper configurations:
JP2: 2-3
JP4: 1-2 (does the jumper need to be removed if using 3.3V?)
JP6: 1-2
JP7: 1-2
JP8: 1-2
JP17: open
JP18: 2-3
JP19: 1-2
JP20: 1-2
JP21: 2-3
JP22: 2-3
JP23: 1-2
JP24: 3.3V power applied to pins 2-3
Is there anything glaringly wrong with this setup?
Thanks in advance