Hello,
I'm looking into the DAC7716 component, I'd like to use it as a 0-20V output, I understand that the supply voltages are as follows: Electricals characteristics:
All specifications at TA = TMIN to TMAX, AVDD = +11V to +18V, AVSS = -11V to -18V, VREF = REF-A = REF-B = +5V, DVDD = +5V, IOVDD = +1.8V to DVDD, AGND = DGND = REFGND-A = REFGND-B = SGND-x = 0V, and DAC gain = 4, unless otherwise noted (PDF page 3)
My question is the following:
1) What is the minimum voltage to use to have an Output from 0 to 20V?
2) Can the Vss value be zero?
Thanks in advance,
Mathieu Z.