Hi
I'm planning to use AFE5816 for data capture. Please share SPI command sequence for IC initialzation and data sampling. Also is there any C code available for the same.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I'm planning to use AFE5816 for data capture. Please share SPI command sequence for IC initialzation and data sampling. Also is there any C code available for the same.
Thanks
Please must refer to the AFE5816 datasheet page 84
10.4 Initialization Set up.
Thank you!
And also refer to the AFE5816 datasheet
page 85 Figure 106 and you can see SPI registers are
setting after powers, RESET, SEN, ADC_CLK are done.
and also refer to User's Guide as well.
Hi Chen Kung
What i'm referring is sequence of SPI register codes to be written or read for initializing the IC.
Please comment.
Hi,
Please and hope you can see the following link:
C:\Program Files (x86)\Texas Instruments\HMC-DAQ GUI\Scripts\AFE5816\QUICK_START\init.cfg
Of course you can see all the code including AFE5816 device SPI's.
Thank you!