Part Number: TSW14J10EVM
I want to use the TSW14J10EVM as intermediary card between the ADC12DJ3200EVM and my KU115 based FPGA platform (not from XIlinx).
I found in the TSW14J10EVM a setup that does not require FPGA jtag connection between FPGA board and TSW14J10EVM:
ADC12J4000EVM With a Xilinx Zynq ZC706 Development Board Setup Example
My approach would be to connect the three boards, assuming the TSW14J10EVM just listens in on the FMC JESD204B signals, and can export over USB to visualize the spectrum in the HSDC Pro GUI software.
For some reason, the TSW14J10EVM states compatibility with only three FPGA's (Xilinx KC705, ZC706 and VC707 platforms). I don't understand why there would be a compatibility issue as the FMC connection and signals are not FPGA dependent, especially if JTAG is not connected?
Can I use the TSW14J10EVM with HSDC ProGUI as independent man-in-the-middle to both:
- forward the FMC connection the the ADC as if it was not there,
- and to export the JESD204B communications to USB to HSDC software?