This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP92066: What is the different between Specified temperature range and Operating temperature range?

Part Number: LMP92066

As shown in below image, There is a specified temperature range of -25 to 120 degC and an operating temperature as -40 to 125 degC. We need a lower temperature range of till -40degC so just wanted to check on this spec.

  • Hi,

    If you see the electrical specifications table, most of the parameters are specified for -20 to +120 deg C. Where as some parameters are tested up to -40 to +125 deg C.

    This means that device can operate upto -40 to +125 degC. Have a look at the specifications you care about for the operating range and decide.

    Regards,

    AK