This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7573: DAC7573 A0 and A1 input levels

Part Number: DAC7573


I am looking for information about the A0 and A1 inputs of the DAC7573. The datasheet states it can be connected to Vdd or digital ground. If Vdd is 5V, and IOVdd =3.3V, is it acceptable to connect A0 and A1 to Vdd=5V?

Additionally, what is the input impedance, I assume it is high impedance standard input.