Hello,
I would like to connect the SPI programming interfaces of 32 ADC3583 to one FPGA (SPI master).
Is it possible to cascade the 32 ADCs to one daisy chain? So only one SPI interface with one /SS is needed?
BR, Frank
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I would like to connect the SPI programming interfaces of 32 ADC3583 to one FPGA (SPI master).
Is it possible to cascade the 32 ADCs to one daisy chain? So only one SPI interface with one /SS is needed?
BR, Frank
After reading the data sheet, I am able to answer my question by myself:
The chip has noch dedicated pins for MISO and MOSI, but a I/O called SDIO.
So, a daisy chaining is not possible.
Hello Frank,
Due to the bidirectional nature of the 3-wire variant, an I/O expander would be required, with which the Interface group may be better suited to help you:
https://e2e.ti.com/support/interface-group/interface/f/interface-forum
I would suggest posting there and include your data rate because that will likely be a question they'll have.