Hi,
I'm trying to debug a problem with an product using AFE5805s. Sometimes during powerup, the AFE seems to get into a "bad" state where it's noise floor jumps to 60dB (system NF is typically around 15dB). The noise appears to be random although with a high enough input signal I can make out some signal in the noise but it's essentially drowned out. Usually this happens when it's powered on, but I've seen it go into this state after a high amplitude input signal is supplied. Sometimes it will recover after a few minutes but often it does not. Does anyone have any similar experience? Any ideas where I should start looking? Could this be one of the amp stages getting into a positive feedback loop?
Any help is appreciated!