Part Number: ADS7953
Hello,
I am using the ADS7953 and have a question regarding the use of GPIO2 to control the input range. The input range can be selected via GPIO2 or bit DI06 in the mode control registers. What happens if GPIO2 is used to select the input range and the range to be selected differs from what is set in the mode control register? For example, if GPIO2 is tied HIGH to select Range 2 and the mode control bit = 0 to select Range 1.

Thank you.