Hi, I would like to know how much is the input bandwidth (-3dB) could support for SM73201.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello JJ,
The analog input bandwidth is primarily limited by the sample switch resistance (R-sample=200ohm) and the sampling capacitance (C-sample=20pF). You can find these values in the 'Input Settling' section of the datasheet, along with Figure 34.
The estimated -3dB bandwidth is then f-3dB=1/(2*PI*Rsample*Csample)=39.8MHz
Regards,
Keith Nicholas
Precision ADC Applications