Part Number: ADS1232REF
I ordered a ADS1232REF-Modul to evaluate different bridge circuits.
At first the module was working fine when I powered it with a 9V Battery. I used a weak battery and it became empty very quick, so the module turned off. Now after replacing the empty battery with a new one the module does not power up. I checked the battery power to make sure its at 9V, also I tried an external power supply at 9V.
At all test points on the module ( Vref+, 5V, 3.3V) I only measure 0.2V against GND.
Is it possible to get an replacement for the board or is this a known error?