Hello team,
I have a quick question if the DAC43608 digital input range may not cover the I2C VIL specification.
We can find that the DAC43608 accepts VIL up to 0.5V.
On the other hand, the I2C spcification defines VIL as up to 0.3xVDD as follows.
For example, when the VDD is 3.3V, the I2C should be able to accept up to 0.99V as the input low.
Does it mean that the DAC43608 can't accept the I2C stardard for the VIL in all VDD range or can we expect to take some voltage margin at higher VDD(e.g. 3.3V)?
Regards,
S.Sawamoto