Part Number: ADS7947
Unlike some of TI’s ADC datasheets, the datasheet for the ADS794x series provides no maximum input current specification. This is probably a big hint that I’m approaching my problem the wrong way, but perhaps somebody will give me a nudge in the right direction.
I’m designing an add-on front end for an existing circuit based on the ADS7947. This circuit uses 3V for AVDD, but input will be provided by an op-amp with a +/-5V supply. Under normal operating conditions this amp will be outputting a voltage that’s safely between 0V and AVDD, but the order of power rail ramp up/down and other events may result in the amp’s output voltage being momentarily outside of this range. My first thought was to simply place a BAT54-type Schottky array in front of the ADC to clamp input to between 0V and AVDD +/- diode Vf, with current-limiting resistors on either side, but I can’t feel good about that if I don’t know what current I’m trying to keep it under.
Any advice would be much appreciated!
~Aaron