This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8812: Maximum value of current supplied to VREF pin

Guru 12065 points
Part Number: DAC8812

Hi,

What is the maximum current required to supply the VREF pin?

Thanks,

  • Hi Koki,

    The reference input resistance is 4kΩ min or 6kΩ max. The current required by your reference will depend on the voltage of your reference. If you are using the ±15V range then the reference will need to be able to regulate ±15V at least ±3.75mA. 

    Best,

    Katlynne Jones