Depending on the situation, I'm changing DAC Output level from 5.1V to 2.5V, and vice versa.
How can I change this DAC Output level gradually?
As-is: Please refer to only blue wave.

To-be:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Depending on the situation, I'm changing DAC Output level from 5.1V to 2.5V, and vice versa.
How can I change this DAC Output level gradually?
As-is: Please refer to only blue wave.

To-be:

Hello,
You can set the slew rate in the GENERAL_CONFIG Register:

Set the high and low data values in the DAC_MARGIN_HIGH and DAC_MARGIN_LOW Registers:


Then you can slew between the high and low values using the external GPI trigger or the software trigger in the PMBUS_OPERATION Register:

Best,
Katlynne Jones
Hello, I'm a co-worker with her.
First of all, I'm wondering if pmbus bit is right as mentioned in the datasheet.
I run like this
Reg: 0xD1, Val: 0x1204 // PMBus enable, slew rate 25us
Reg: 0x25, Val: 0x0960
Reg: 0x26, Val: 0x03C0
Reg: 0x01, Val: 0xA400 --> i2c fail (Can't access reg 0x01)
Reg:0x21 Val: 0x0960
But,
Reg: 0xD1, Val: 0x0204 // PMBus Disable, slew rate 25us
Reg: 0x25, Val: 0x0960
Reg: 0x26, Val: 0x03C0
Reg: 0x01, Val: 0xA400 --> i2c success
See if slew rate is working --> not working.
Reg:0x21 Val: 0x0960
So, Please help me with how to get through this.
Wrap up)
1) pmbus bit 0 in 0xD1 --> can control i2c addr 0x01 (it's not the same with the datasheet)
2) addr 0x01 success, but then slew rate is not working
Hello,
Do not enable PMBUS if you are using I2C. PMBUS is an alternate communication standard that the device can uses. I did make a mistake though. The software trigger is in the TRIGGER register in the PMBUS_MARGIN_HIGH and PMBUS_MARGIN_LOW fields, not the PMBUS register:

Instead of Reg: 0x01, Val: 0xA400, it should be: Reg: 0xD3, Val: 0x0800 for a margin high trigger. Let me know if this works for you.
Best,
Katlynne Jones