Other Parts Discussed in Thread: TIDA-010057
We finally have our own SWAROOP board in hand (took a while to get the components !), as well as the TIDA-010057 power supply (MED1427).
However I am having trouble performing the tests described in the SWAROOP user guide.
1) We checked all the power rails: very nice and clean (with 5V on the Green-Power J1-39 pin).
2) We check the SF3 and programed it with the supplied example code (swaroop_v0.1.img).... we programed via RAM as R21 is in, preventing EEPROM reload)
3) We programed the JTAG (FPGA) EEPROM via Vivado with "Swaroop_june.bit" successfully
4) We run HSDC, and select the board.,
5) We select the ADC (AFE5832LPTX), and it launches the AFE5832LPTX 3LVL EVM software.
6) We press "DUT HW Reset", "Initialize Device" and "FPGA reset", and the scripts appear to load.
7) We set the TX channels to 32, and RX channels to 32
But with Trigger Capture both "on" or "off", we cannot get a sync pulse on TP1 (which we should according to the "manual").
What have we missed?
Am I supposed to "Download firmware" in the HSDC software?
Also It appears to write to the FPGA, but when reading it appears non-responsive.
Possibly I am just missing a setting somewhere......
Is there another testing manual I have missed?
How long does the Register Map Configuration take to be read (in full) normally?