This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC3162EVM: Timing with Internal Clocking

Part Number: DAC3162EVM
Other Parts Discussed in Thread: DAC3162

Hi Team, seeking for assistance.

I tried to drive the DAC3162 with an FPGA @ 200MHz. The DAC input is switched from 0x000 to 0xFFF and vice versa at every clock edge to check the full resolution.
I tried to generate the DAC data (DDR format ) as shown in the figure Data transmission format and I send a clock signal 200MHz, Vrms = 0.56V
In attached the input clk and the measured outputs signals (you can check also the simulation signals sended to FMC connector of my FPGA)

I need any suggestion to adjust the timing with internal clocking. As infomation, dac is controlled over a fpga. In attached the received clk from DAC3162 and also the two output signals of the dac.

/resized-image/__size/640x480/__key/communityserver-discussions-components-files/73/InputCLK_5F00_J9.jpg

/resized-image/__size/640x480/__key/communityserver-discussions-components-files/73/waveform-_2800_1_2900_.png

Thank you.

-Mark