Hi expert,
My customer is using ADC161S626.
They give the IN- and IN+ almost the same voltage 2.5V, So the output should be about 0V.
and they try a twice 16bit read and a three times 8bit read to read the data.
however, they found the data changed too much.
you can see the waveform below.SPI clock is 5MHz. since the CS is always low. so it will not enter another AD convert,am I right?
below 2 waveform are all 0V input but the data is totally different.
Does this method not right? however, customer use this method in another project and it works well.
or the SPI clock interval is too long?
The host is IMX6ULL and running linux system. The SPI is configured as below:
BR
Emma