Hi,
According to the data sheet, the lower limit of the update rate is 125Msps, is this the lower limit of the Max update rate?
Customers use it at lower data rates. Is there a lower limit of Update rate specification?
And T1 and T2 of the timing diagram are TYP 3ns. Since T1 + T2 is an update rate, if there is a lower limit for the update rate, please tell us about the maximum values for T1 and T2. I think this is related to the acceptable duty ratio, but I couldn't find it in the DS.
Also, I think that these parameters are usually defined by Min values.
Does TI have the data?
Data Setup Time
Data Hold Time
In addition, these parameters require a Max value.
Propagation Delay Time 1 ns
Output Settling Time to 0.1%
Please tell us about the above parameters if possible.
Regards,
Hiroshi