This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC3283: DAC3283

Part Number: DAC3283
Other Parts Discussed in Thread: CDCE62005,

Hello,


 I am using custom board which has an interfaces of  DAC (DAC3283 ) and Clock Synthesizer (CDCE62005).

For DAC it is 16 bit with 800MSPS DAC output and 8-Bit Input LVDS Data Bus .

I need to give 8 pair of differential input D[7:0]P/N .

My doubt is whether  i need to separate input data as I and Q before given to a actual DAC input OR can i give direct differential pair dac input using DDS compiler with OBUFDS ???