Hello,
I'm working with the ADS112C04. I have a device that will at most output 80mV. Therefore, I can tune the PGA gain fairly high to improve resolution and reduce noise. The current output as measured by a volt meter is 50 mV. At gains 1, 2, 4 I see 50 mV from the ADC but at gain 8, I start seeing 32 mV. At gain 16, I start seeing 19 mV.
Is there a different formula to calculate the output for gains above 4? I see some suggestion of this in the datasheet on page 24, but I'm not entirely clear on this.
Thanks!
Siddharth