Part Number: ADS7957
Other Parts Discussed in Thread: STRIKE
Hi Team,
My customer found after applied 15kV air discharge and 5kV contact discharge ESD test, the output is FFC, even with input shorted to ground.
They tried two ways below, both can help the device recover:
1. write 1 to DI09 to soft reset the device, output is back to normal
2. set DI08 to1 and pull high GPIO3 to keep ADC in active mode, the output is always normal even after the ESD even
What do you think the possible issue it is? Is it any possible way to set the device in power down mode during ESD?
If set DI08 to 1 and pull GPIO3 to high can solve this problem, is there any potential risk for this setup?
Thanks,
Cera