This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS42JB49: JESD204b Frame Assembly

Part Number: ADS42JB49

I'm a new user of JESD204b interfaces. My question is with respect to Table 6 from the ADS42JB49 datasheet. My application need only use 1 input channel of the converter at 200 MSPS. With this configuration the lane line rate would follow:

Lane line rate = (M x S x N' x 10/8 x FC)/ L

= (1 x 1 x 16 x 10/8 x 200E6)/2

= 2.0 Gbps

This is in compliance with the part specifications maximum SERDES frequency, correct? Or is my calculation incorrect because Table 6 from the data sheet does not indicate M = 1 as a valid parameter for the part?