Other Parts Discussed in Thread: ADS125H02,
Hi There-
I've been working with the ADS125H01 and its sister part ADS125H02 in a load cell application. I have 12V, 5V, and 3.3V available on my board, and the load cell is excited at 12V so the two nodes being measured will typically be at 6V each. I'm planning on connecting the HV_AVdd to +12V and I'd like to connect the HV_Avss to 0V as shown below. Is that acceptable for this IC?
Thanks!
Dave