This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298: Maximum temperature in the solder tip

Part Number: ADS1298

Hi Experts,

Please help confirm, what is the maximum temperature that customer can use in the tip of the solder for a rework of a PCB with those components?
He do not mean the temperature of the oven but the one used in a soldering station to do a manual rework.

Can he use MSL Peak Temp(Level-3-260C-168 HR) as the max temp? Otherwise, please advise.

OPN:  ADS1298CZXGT

Kind regards,
Gerald