Other Parts Discussed in Thread: DAC81408, DAC81404, DAC8228
Hello support team,
I am looking for the 14/16 bit DAC resolution with octal simultaneous channel with 1 MSPS sample rate with output voltage range of 0-10 V.
I have found one suitable octal channel DAC with sample rate of 1 MSPS , which is DAC80508. for which i have below queries
1. As in order to have 0 -10 V output voltage range , If I use external reference of Vref =5 V, It is possible to get the output voltage range of 0 -10 V , right?
(with Div setting: 1, gain setting: 2, DAC output range: 0 to 2 x Vref)
2. As our requirement of sampling rate is 1 MSPS , and for DAC sampling rate depends on both settling time and update rate. so for larger voltage variations, such as 0 to 10 V step, settling time would be degraded? and based on that sampling rate will also reduce?
3. Can you please also suggest that 1 MSPS sampling rate is simultaneous for all DAC channels? right?
4. Based on our requirement, DAC Sample rate =1 MSPS, octal or quad channel , output voltage range: 0-10 V , DAC resolution: 14 or 16 , Can you please verify and suggest that the DAC80508 would be suitable or else please suggest other part number?
Awaited our positive feedback.