Hello !
Please advise.
I am trying to synchronise three ADS1287 under the following conditions, but the DRDY outputs are output at different timings.
My image is that all DRDY will output at the same timing when operating in Continuous-sync mode, but is this a misunderstanding?
Currently, the output of DRDY seems to be determined by the timing of initialising AD.
- AD_CLK and SYNC divided from a common clock.
AD_CLK: 819.2 kHz
SYNC: 100 Hz
Sampling: 100 sps
- The rising edge of SYNC is synchronised with the falling edge of AD_CLK.
- The same AD_CLK and SYNC are used for all three channels.
- The setting is Continuous-sync mode.
- However, the DRDY timing of each channel is different.
- The conversion result for each channel is OK.
- It would be perfect if the phases of each CH were aligned.
Thank you,
Akihiro Yamazaki