Part Number: DAC80504
Hi Team
There are two question hope can get your support
1、What's the default state of CRC function, on or off?
2、When the CRC function is turned on or off, will the data input to the DOC be different?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC80504
Hi Team
There are two question hope can get your support
1、What's the default state of CRC function, on or off?
2、When the CRC function is turned on or off, will the data input to the DOC be different?
Hi Harry,
The default state is CRC disabled.
Follow this write cycle (table 4) with CRC is enabled. The 16-bit data written to the DAC is the same, but the total cycle has 32 clocks instead of 24 because the 8 CRC bits are added to the end of the cycle.

The write cycle looks like this (table 2) when CRC is disabled:

Best,
Katlynne Jones