This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8904B: VREF above RVDD - 0.3V

Part Number: ADS8904B

Hi,

For a variety of reasons, I would like to be able to use the same voltage rail (= 3.3V) that supplies the RVDD input to supply the VREF input as well. I realize this would violate the maximum recommended voltage for the VREF input according to the datasheet, but I would like to understand what impact this might have for functionality and/or performance?

Regards,
James