Hi team,
I refer this post [How do I convert ADC output codes to volts?] and convert ADC output code to volts, and, for test signal, yes, got expected result,but got an unexpected rusult when feed a simulator signal.
Please give me some hands, thanks.
Test signal setting:
Data Rate = 125 SPS Input signal voltage & freq: +/-1mV, 1Hz Ouput range: -1mv ~ 1mV
Simulator Signal:
Data Rate: 125 SPS Input Signal voltage & seq: +/-1mV, 2Hz Output range: 0.75mV ~ 1.75mV
for simulator signal, i have no idea if the output range should be about -1mV ~ 1mV ??
test signal@1Hz, 1mV screenshot:
simulator square signal@1mV, 2Hz:
simulator ecg signal@ 1mV:
Best regards,
Gavin