Is a Verilog, SystemVerilog, or VHDL simulation model available for the ADS8168? That would be helpful to speed up debug and do a more thorough verification of my interface RTL.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is a Verilog, SystemVerilog, or VHDL simulation model available for the ADS8168? That would be helpful to speed up debug and do a more thorough verification of my interface RTL.
Hello Brett,
Welcome to the TI E2E community!
Unfortunately, we do not have any kind of digital simulation model for the ADS8168. I typically recommend starting with the default SPI-00 with single SDO to verify basic functionality, and then move to the different interface protocols if needed.
If you run into problems, feel free to post screenshots of the interface signals (logic analyzer or scope) and I can help debug.
Regards,
Keith Nicholas
Precision ADC Applications
Is a Verilog, SystemVerilog, or VHDL simulation model available for the ADS8168? That would be helpful to speed up debug and do a more thorough verification of my interface RTL.
This is an evergreen question.
What TI (and Analog Devices, and the others) fail to understand is that FPGA engineers really need to verify their designs. To do that, we need models that are correct. We can certainly create our own models from the data sheets (and we do; I have a good couple dozen right now) but the problem is that the assumptions we make in writing our design HDL are the same as those we make to create the model. And if those assumptions are wrong, then we waste time in the lab verifying operation and correctness.
Come on, TI, it's mid 2022, and your high-speed converters are meant to interface with an FPGA. Models we can trust are mandatory.
At least the response was not, "We have IBIS models ..." -- I've actually been told that by a tech support person.
Hello Brett,
I am glad you were able to get everything working.
Brett, Andy,
Thank you for the suggestions regarding an HDL model for the interface. This is not something that we have provided in the past, but we will certainly consider this in the future.
Regards,
Keith