Part Number: TSW1400EVM
Other Parts Discussed in Thread: ADS4249EVM, ADS4249
hello staff
I had this problem after testing with TSW1400EVM

According to the communication with some staff, the problem is generally concentrated in the power supply part.
I use the Agilent E3632A power supply here, with a power supply range of 0-15V 7A channel. When powering the TSW1400EVM, the current is always kept at around 0.38A at a voltage of 5V, which is too far from the 4A current in the manual.
According to some posts, the power supply cord has also been replaced, but there is still no progress. May I ask what could be the problem?
In addition, after I use HSDC Pro to download fireware to TSW1400EVM, the current of the board can be maintained at 1.1A, which seems to indicate that the hardware is not broken, but it still cannot reach the level of 4A.