We have the mikroe adc 15 board for testing and after setting everything up I started noticting only the irst readings were valid.
After ~1.96seconds the board resets and we get 0xFF22 indicating a succesful reset.
This seems to be also happening even if I dont configure any registers.
I leave everything at default, send NULL in a loop every 100ms and still get a a 0xFF22 at the same frequency.
With configuring adc:
Currently dont have a picture without conifiguring it, will upload it later if necessary,
but in that case the first response from the ADC is 0xFF22,
subsequent responses are 0x500 until the next drdy signal after which I get one 0xFF22 once again.
Is it possible the adc is faulty?