Hi.
Regarding ADS7828 that is an 8-channel ADC with I2C interface.
If in the schematic I'm going to have 8x 0/4~20mA current inputs using 8x the circuit below, where a 20mA output from sensors do generate 2V at the 100R sampling resistor. From this resistor to the ADC input there is (currently) a 22K current limiting resistor that I wanted to reduce the value due to the analog input leakage, because I'm considering that in the worst case of transient at input "I-IN-1", it could be generated a voltage spike of 65V max over the 100R resistor during some microseconds. I suppose that there exist internally to ADS7828 analog pins a clamping diode to a positive rail (yes/no?). My question is if that rail is the VCC pin or the VREF voltage. And if I could know what is the maximum current (estimated) that can flow through the internal diode, if it does exist. Initially I plan to use the internal 2.5V voltage reference.
EDIT: The TBU device can take a maximum of 1us to actuate, according to the datasheet.
Regards,
Jeferson.