This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ5200RF: Link up in JMODE5, 7, 11, 22 etc other than JMODE0/2

Part Number: ADC12DJ5200RF
Other Parts Discussed in Thread: ADC12DJ3200

#1

We are using ADC12DJ5200 as a drop-in replacement of ADC12DJ3200 because we like to run at higher rate or Fs. 

#2

Our current FPGA project is in JMODE0/2 at Fs = 1600MHZ so Fbit = 6400Mbps. The rxlink_clk = 160MHz (or 6400/40)

The FPGA project was derived from TI Arria10 + ADC12DJ3200 JMODE0 Design Firmware — SLAC748.ZIP

#3

I got ADC12DJ5200 work with the current FPGA project so no question about JMODE0/2.

#4

However i could not get link up nor device aligned after changing to JMODE5/7.

Where Fbit = 6400Mbps so Fs = 2560MHz as R = 2.5. The rxlin_clk = 160MHz as the Fbit is the same. 

Were they right?

#5

I changed F = 1, S = 4, N= N' = 8 and K = 20 for the FPGA IP core, while L and M stay. 

Did I miss anything?

#6

Obviously, L and M definitions for the IP core configuration differ from what's in the ADC datasheets.  

The L = 8 and M = 2 for the FPGA IP core configuration from Arria10 + ADC12DJ3200 JMODE0 Design Firmware

Which is for JMODE0/2. 

So I like to know what would be the proper values of L, M, K, F, S etc. for JMODE 5/7 and JMODE11. 

Hope to hear from you ASAP. Thanks a lot.