This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7138: Acquisition time

Part Number: ADS7138


I wanted to know if ADS7138 increases acquisition time when lowering the sample rate. I can not find information about his in the datasheet. I can only find die minimum acquisition time. The reason why I am asking is to determine the requirements for the driving circuit so that the input is settled within the acquisition time.

  • Hi Lidong,

    With a lower sampling rate, the ADS7138 enables longer acquisition time. This is because the conversion time of ADS7138 is fixed and it is specified as tCONV in the switching characteristics table.

    Regards,

    Rahul