The offset for the PGA, typical and max are very different, under what conditions does the max offset occur.
Also when bypassing the PGA I assume the S/H cap is driven directly by the inputs. What is the size of the S/H caps and aperture time for 20 sampl,es per sec so I can see what effect the source impedance has. We have a 10K bridge and 4k7 1n/10n input filter, making a source impedance of 10K on each differential input.. We are seeing 200uV offsets when the PGA is bypassed on some boards and only 30uV when used and are not sure if this is bias current, S/H loading etc.
Thanks