Hi Team,
I have this requirement to measure a high voltage input +/-1000V with an accuracy of 2%.
I selected the AMC1400 which has better creepage and clearance distances.
My question is about interfacing this device with MCU to satisfy measurement requirement. I may have 2 options:
- Convert the output of AMC1400 to a single-ended signal and then connect it to MCU ADC
- Connect to output pf AMC1400 to a differential input ADC and then interface it with MCU using SPI.
I have joined 2 diagrams detailing the 2 options.
Thanks in advance for your support.
Regards,
Abderrahman