Hi,
We are planning in using DAC7822 in one of our project, we intend to use it only on writing mode. So I was wondering if that the L/W control signal could be tied to logic-low(writing mode) all the time, instead of having it to be driven by either an FPGA or microprocessor. This is unclear to me from the Datasheet as in the timing diagram you have a R/W high to CS low timing requirement of 5 ns.